Keysight PNA Hardware and Software Upgrades
Firmware and Software Upgrades for All PNA ModelsWe maintain a comprehensive Firmware and Software web page for all PNA models. Please visit this site for more information. |
|||
Hardware Upgrades
|
|||
PNA HostID UtilityThe new N52xxB model numbers changed to a HostID format which is "model,serial". (For example, "N5247B,US57181234") When upgrading from one N52xxB model to another, the current HostID is used for the initial reset of the model number. For all other PNAs, the HostID is an 8-digit number. When upgrading from one model number to another, a new license entitlement certificate will be issued. When this certificate is redeemed, the automated system will ask for the instrument's Host ID. Be sure to use the new Host ID that is associated with the new model number. Using the current Host ID will cause a license to be generated which will not work with the instrument. To determine the new Host ID, use this utility with the new model number. |