Currently Available NVNA Software

 


Operating System

Latest Production Releases

Latest Customer Releases


Notes

All Windows 7 and Windows 10 PNA-Xs
Note: Minimum Windows 7 firmware is A.10.20.01.
A.02.04.05
(04 Dec 2013)
A.02.10.04
(03 Feb 2020)
  A.02.10.04 requires below FW:
"B" models: >A.13.80.12
"A" models: >A.10.65.03
All Windows XP PNA-Xs
Note: Maximum Windows XP firmware is A.09.99.99.
A.02.00.03
(24 Mar 2011)
A.02.04.10
(23 Jul 2015)
See compatibility note below.
  Production releases are fully supported. Customer releases are newer versions that are also fully supported.  

  • NOTE: S935xxB licenses require NVNA version A.02.10.03 or higher.
  • NVNA version A.02.04.02 (or higher) requires PNA firmware revision A.09.90.01 or above.
  • If not already installed, the Matlab RunTime 7.14 is also required. Download this 180MB file and install it on the PNA.
    PNA's shipped after mid 2011 should already have this installed.
  • Compatibility between 1.xx and 2.xx: Recalled 1.xx states with external instrument parameters may not be fully imported. Variable values may need to be re-entered.

If you have Option 521 or S94521A/B, you must perform the following steps:

  1. For "B" model instruments only, check IO library version. If not already installed, download and install IO Libraries Suite 2018 Update 1.0 or greater.
  2. Download and install this MTune utility on the PNA.
  3. Download this Maury driver and place it in the directory:   C:\ProgramFiles (x86)\Maury\MTune\Driver


NVNA Help

The User and Programming manual for the NVNA.

NVNA Help is available in the following three formats:

  1. Online - Click to view the latest. Links to PNAHelp do NOT work.
  2. Offline - Click to download NVNAHelp.chm to your PC. (13 MB). This file is embedded in the NVNA. See Problems viewing the .chm file? (below)
  3. Printable - Click to immediately download to your PC. (14 MB). Then print all or some of the file.

Problems viewing the .chm file?

  • To view NVNAHelp.chm, save the file to your hard drive.
  • For Windows XP, right-click on the file, click Properties, then click Unblock.

Other Documentation

Last Updated: Feb 04, 2020