Write/Read
About Linear Frequency Sweep

StopFrequency Property


Description

Sets or returns the stop frequency of the channel. (Channel Object)

Sets or returns the stop frequency of the segment. (Segment Object)

Sets or returns the stop frequency of the FOM Range. (FOMRange Object

Sets or returns the stop frequency of the Power Sensor coverage (GuidedCalibrationPowerSensor Object)

Sets or returns the stop frequency of the Phase Reference Calibration.

See also Measurement2 interface.

 VB Syntax

object.StopFrequency = value

Variable

(Type) - Description

object

Any of the following:

Channel (object)

Segment (object)

FOMRange (object)

GuidedCalibrationPowerSensor (object)

PhaseReferenceCalibration (object)

value

(double) - Stop frequency in Hertz. Choose any number between the minimum and maximum frequencies of the analyzer.

Return Type

Double

Default

Channel - Maximum frequency of the analyzer.

Segment - 0

FOMRange - Maximum frequency of the analyzer.

GuidedCalibrationPowerSensor - Maximum frequency of the analyzer.

PhaseReferenceCalibration - Maximum frequency of the analyzer.

Examples

chan.StopFrequency = 4.5e9 'sets the stop frequency for the channel object -Write

stopfreq = Chan.StopFrequency 'Read

C++ Syntax

HRESULT get_StopFrequency(double *pVal)

HRESULT put_StopFrequency(double newVal)

Interface

IChannel

ISegment

IFOMRange

IGuidedCalibrationPowerSensor