Frequency range is the span of frequencies you specify for making a device measurement.
See other 'Setup Measurements' topics
How to set Frequency Range |
|
There are two ways to set the frequency range:
|
|
Using front-panel |
PNA Menu using a mouse |
|
|
For PNA-X models |
|
|
|
Start Specifies the beginning frequency of the swept measurement range. Stop Specifies the end frequency of the swept measurement range.
|
Center Specifies the value at the center of the frequency sweep. This value can be anywhere in the analyzer range. Span Specifies the span of frequency values measured to either side of the center frequency. |
Zoom allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep.
Zoom operates on the Active Trace and all traces in the same channel as the active trace, regardless of the window in which they appear.
How to Zoom in a measurement window |
Zoom - changes the channel stimulus settings to the left and right border values of the Zoom selection Zoom xy - changes the channel stimulus settings as above. In addition, the Y-axis scale of the active trace changes to the approximate scale of the Zoom selection. Zoom Full Out - changes the channel stimulus settings to the full span of the current calibration. If no calibration is ON, then the stimulus settings are changed to the full span of the PNA model. Notes
Zoom is NOT available for the following:
|
Measurements with a CW Time sweep or Power sweep are made at a single frequency rather than over a range of frequencies.
How to set CW Frequency |
|
You can also set CW frequency from within the Sweep Type dialog box. |
|
Using front-panel |
PNA Menu using a mouse |
|
|
For PNA-X models |
|
|
|
|
CW Type a value and the first letter of the suffix (k,m,or g) or use the up and down arrows to select any value within the range of the PNA. |
The resolution for setting frequency is 1 Hz.
The frequency range of the PNA covers several internal frequency bands. The higher the frequency range of the PNA, the larger the number of bands. The source power to your DUT turns off as the stimulus frequency is swept through these band crossings. To learn more, see Power ON and OFF during Sweep and Retrace.
The listed frequencies in the following tables are the stop frequency of the specified band, and the start frequency of the following band.
Frequency band crossings are different for the following models:
For 3 GHz, 6 GHz, and 9 GHz (discontinued) PNA models:
Band |
Frequency |
1 |
10 MHz |
2 |
748 MHz |
3 |
1500 MHz |
4 |
3000 MHz |
5 |
4500 MHz |
6 |
6500 MHz |
For E8362 / 63 / 64 A/B
(A models do not have band 0)
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
.045 |
|
|
|
|
1 |
0.748 |
9 |
7.60 |
17 |
25.60 |
2 |
1.500 |
10 |
10.00 |
18 |
30.00 |
3 |
3.00 |
11 |
12.00 |
19 |
32.00 |
4 |
3.80 |
12 |
12.8 |
20 |
36.00 |
5 |
4.50 |
13 |
15.20 |
21 |
38.40 |
6 |
4.80 |
14 |
16.00 |
22 |
40.00 |
7 |
6.00 |
15 |
20.00 |
23 |
45.60 |
8 |
6.40 |
16 |
22.80 |
24 |
48.00 |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
.045 |
9 |
10.00 |
18 |
32.00 |
1 |
0.748 |
10 |
12.00 |
19 |
36.00 |
2 |
1.500 |
11 |
12.80 |
20 |
40.00 |
3 |
3.00 |
12 |
15.40 |
21 |
44.70 |
4 |
3.80 |
13 |
16.00 |
22 |
46.20 |
5 |
4.00 |
14 |
20.00 |
23 |
51.20 |
6 |
4.50 |
15 |
24.00 |
24 |
60.00 |
7 |
6.00 |
16 |
25.60 |
25 |
64.00 |
8 |
7.70 |
17 |
30.00 |
|
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
1 |
.045 |
11 |
10.500 |
21 |
28.600 |
2 |
.748 |
12 |
12.500 |
22 |
31.250 |
3 |
1.5 |
13 |
15.750 |
23 |
31.500 |
4 |
3.125 |
14 |
16.667 |
24 |
33.333 |
5 |
4.167 |
15 |
18.750 |
25 |
37.000 |
6 |
5.250 |
16 |
21.000 |
26 |
40.500 |
7 |
6.250 |
17 |
22.500 |
27 |
41.667 |
8 |
7.875 |
18 |
25.000 |
28 |
42.000 |
9 |
8.333 |
19 |
26.250 |
29 |
46.800 |
10 |
9.375 |
20 |
26.500 |
30 |
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
.00112 |
9 |
8.333 |
1 |
0.010 |
10 |
9.800 |
2 |
0.040 |
11 |
10.500 |
3 |
0.748 |
12 |
12.500 |
4 |
1.500 |
13 |
15.000 |
5 |
3.125 |
14 |
15.750 |
6 |
4.166 |
15 |
16.666 |
7 |
5.250 |
16 |
18.750 |
8 |
6.250 |
17 |
20.100 |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
.396 |
24 |
8.50 |
1 |
Reserved |
13 |
.500 |
25 |
10.664 |
2 |
.014 |
14 |
.628 |
26 |
12.00 |
3 |
.019 |
15 |
1.00 |
27 |
12.80 |
4 |
.027 |
16 |
1.50 |
28 |
13.51 |
5 |
.038 |
17 |
2.00 |
29 |
15.40 |
6 |
.053 |
18 |
3.00 |
30 |
16.00 |
7 |
.075 |
19 |
3.20 |
31 |
18.00 |
8 |
.105 |
20 |
4.00 |
32 |
20.00 |
9 |
.146 |
21 |
5.32 |
33 |
21.328 |
10 |
.205 |
22 |
6.75 |
34 |
22.50 |
11 |
.250 |
23 |
8.00 |
35 |
24.00 |
Last modified:
10/23/06 |
MX Added new band crossings |
10/16/06 |
Moved phase lock lost indicator |
9/12/06 |
Added link to programming commands |
9/27/06 |
MX Added UI |