Keysight PNA Series Hard Disk Drive Part Numbers

 

Determine Your CPU Board

Keysight has shipped seven different CPU boards with the PNA family over the past twelve years. Each CPU board has different boot-up and hard drive format requirements. So Keysight supplies several hard disk drives which are imaged to work with the various combinations of CPU hardware and Microsoft Windows operating systems. To find the correct hard drive part number, find your CPU board type from this list, then find the hard drive part numbers in the table below.

  • 266 MHz Pentium -- this board has one USB port oriented horizontally and a single GPIB port.
    (Shipped only with the E8356A/57A/58A until February 2002. This board is now obsolete.)
  • 500 MHz Pentium III -- this board has one USB port oriented vertically and a single GPIB port.
    (Shipped on various PNA models from November 2001 to April 2006. This board is now obsolete.)
  • 1.1 GHz Pentium M -- this board has four USB ports and two GPIB ports.
    (Shipped on various PNA models from April 2006 to the present.)
  • 1.6 GHz Pentium M -- PNA-X only. This board has a non-removable internal hard drive.
    (Shipped on the N5241A/42A PNA-X until September 2009. This board is now obsolete.)
  • 2.0 GHz Core Duo -- PNA-X only. This board has an ejectable hard drive.
    (Used on all N5244A/45A/64A models until Nov 2011. Used on N5241A/42A from September 2009 to Nov 2011.)
  • 2.0 GHz i7 -- All N524xA PNA-X and all N522xA PNA from Nov 2011 to Dec 2015. This board has an ejectable hard drive.
  • 1.87 GHz Celeron -- All PNA-L (N5231A thru N5239A) from July 2012. This board has an ejectable hard drive.
  • 2.2 GHz -- All N524xA PNA-X, all N522xA PNA, and all N5231A thru N5239A PNA-L from Dec 2015. This board has an ejectable hard drive.
Pictures of the CPU boards can be seen here.


Determine Your Hard Drive Part Number

From the very first PNA shipped in October 2000 until January 2009 (Sep '09 for some models), PNAs were shipped with PATA (Parallel Advanced Technology Attachment) interface hard drives. These hard drives have become obsolete in the industry, and Keysight is now producing PNAs with SATA (Serial Advanced Technology Attachment) drives. We have a supply of PATA drives to support our RF PNAs which are not easily convertible to the SATA interface.

The table below shows the PATA and SATA part numbers for the various CPU configurations. If the PNA being serviced is an E8356A/57A/58A, E8801A/02A/03A, or N3381A/82A/83A, see note 5 below.

The 266 MHz and 500 MHz CPUs and the Windows 2000 Operating System are no longer supported. Please contact us for information on upgrading these systems.

Ordering one of the ten digit part numbers shown here will get you a fully imaged hard drive containing the Windows operating system and the latest PNA firmware. Order one of these parts if you are replacing an identical drive.

The N898xA model numbers shown here should only be ordered when upgrading from one operating system to another. The N8980A/81A/82A, which are now obsolete, were sold as a Windows 2000 to Windows XP upgrade drive. The N8983A/84A are Windows XP to Windows 7 upgrade drives. These include a new Windows Certificate of Authenticity sticker and a fully imaged hard drive mounted in a "cradle" with the necessary interface boards. If you are not upgrading the operating system, order the ten-digit part number shown in the table below for your CPU board.

CPU Type & Part Num. 266 MHz Pentium 500 MHz Pentium III 5 1.1 GHz Pentium M 5


E8364-60204
1.6 GHz Pentium M

N5242-60037
2.0 GHz Core Duo
W1312-60068
W1312-60190
2.0 GHz i7


W1312-60196
1.87 GHz Celeron

W1312-60297
2.2 GHz


W1312-60211
System CPU Version 1.0 2.0 3.0 4.0 5.0 6.0 6.1 7.0
Associated
PNA Models
E835xA E835xA,
E836xA/B
N5230A
E836xA/B,
N5230A
E836xC,
N5230C
N5241A/42A N524xA N524xA, N522xA N5231A-39A N524xA, N522xA, N5231A-39A, N5264A N524xB, N522xB, N5231B-39B, N5264B
Windows XP
Operating
System
Not
supported
Obsolete SATA part number was E8801-60070 2

Obsolete PATA part number was E8801-60063

The N8980A is now obsolete.1
E8364-60192 3
(E8364-10002 on disk label)

Obsolete PATA part number was E8364-60190

The N8981A is now obsolete.1
N5230-60050 3
(N5230-10049 on disk label)

Obsolete PATA part number was N5230-60048

The N8982A is now obsolete.1
N5242-60035 2
(PATA interface)

This drive is discontinued. Contact Keysight. 2
N5242-60044 4


This drive is discontinued. Contact Keysight. 2
N5242-60088 4



HDD S.09.xx
N5235-60060 4
Not
supported
Not
supported
Windows 7
Operating
System
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
N8983A 4, 7

N5242-60132
N8983A 4, 7

N5242-60132
N8984A 4, 7

N5242-60133

HDD S.28.xx
N5242-60134 4



HDD S.32.xx
Windows 10 10
Operating
System
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
Not
supported
N8985A 4, 8

N5242-60135

HDD S.40.xx
Drive
Capacity 6
Not
supported
40 GB 80 GB 80 GB 40 GB 80 GB 80 GB/
256 GB 9
80 GB/
256 GB 9
80 GB/
256 GB 9
120 GB/
256 GB 9

Notes:

  1. The N8980A/81A/82A are obsolete. These assemblies were intended for Windows 2000 to Windows XP upgrades. New Windows XP licenses can no longer be sold.
  2. The E8801-60070, N5242-60035, and N5242-60044 are no longer orderable from Keysight. Please contact us to discuss options for migrating to a newer CPU and solid state drive.
  3. The E8364-60192 and N5230-60050 are under inventory control. These drives may be restricted to those customers who have already purchased extended support contracts. If you require a replacement for a PATA drive, you will need to order the applicable SATA hard drive part number and the N5230-60052 hard drive carrier kit. This kit contains a collection of all the parts required to assemble the hard drive carrier for the SATA drive. Please note that the N5230-60052 will not work with a PATA drive.
  4. This solid state drive includes (and is already mounted to) the slide-out drawer that fits into the CPU assembly.
  5. The part numbers in the columns for the 500MHz and 1.1GHz CPUs apply to PNA models E836xA/B/C and N5230A/C. PNA models E8356A/57A/58A, E8801A/02A/03A, and N3381A/82A/83A can not be converted to use a SATA drive. Please contact us to determine if a replacement PATA hard drive is available.
  6. The hard disk drive (HDD) or solid state drive (SSD) capacities shown above are the total writeable partition size for each drive. The total base drive capacity is often larger since the industry continues to evolve and Keysight must migrate to larger drives. Keysight does not change the partition sizes for a given drive image, even when it is put on a larger capacity drive.
  7. The N8983A and N8984A models are ordered when upgrading from Windows XP to Windows 7. These models include the N5242-6013x drive shown associated with these models and a Microsoft Windows 7 Certificate of Authenticity sticker.
  8. The N8985A model is ordered when upgrading from Windows 7 to Windows 10. This model includes the N5242-60135 drive shown associated with this model and a Microsoft Windows 10 Certificate of Authenticity sticker.
  9. The 256 GB drive (intro Aug 2020) is partitioned as:- C: 120 GB System; D: 73 GB Userstore; E: 10 GB Datastore; F: 35 GB Recovery
  10. Keysight will always use the Long-Term Servicing Channel (LTSC) [formerly, Long-Term Servicing Branch (LTSB)] version of Windows 10. Microsoft has released versions 1507, 1607, and 1809 for the LTSC. (Reference) From October 2018 to the end of 2020, Keysight has shipped the PNA hard drive with version 1607. We will transition to using version 1809 in the next few months.


Other Alternatives

An ESATA SDD adapter tray is available for the N524xA/B PNA-X models with CPU Version 5, 6, or 7, the N522xA/B PNA models, and the N5231A/B-N5239A/B PNA-L models with Windows 7. The part number is W1312-60070. See our security web page for more information.

This ESATA adapter tray does not work with Windows 10.

esata_tray_sml (11K)


Last Modified: 06 April 2020