Welcome to the software downloads page for N1500A Materials Measurement Suite, 85070E Dielectric Probe Kit and 85071E Materials Measurement Software
N1500A Materials Measurement Suite
Important! Please read before installing:
• Runs on Windows XP, Windows 7, Windows 8, and Window 10
• Please see N1500A Supported Analyzers for model and firmware requirements.
• If installing the N1500A free trial over a previous installation of 8507x software, the 8507x software will be uninstalled. Please make sure you have access to 8507x series installation files if you intend to go back after the trial period. 8507xE version files are available in the right hand column.
Install includes software with embedded help file, latest FlexLM driver, and free two week trial license.
Web Help lets you instantly view the very latest information online.
Software Release Notes
If installing N1500A on an external PC, Keysight IO Libraries are required to connect to an analyzer. Install IO Libraries only on the PC. Do not install IO Libraries on the analzyer.
• Download Keysight IO Libraries here
|